BACnetObjectBase.GetBACnetArraySizeOfTwoProperties (METH)
METHOD GetBACnetArraySizeOfTwoProperties : CmpBACnet.IEC_BACNET_STATUS
Returns the minimum number of elements in two BACnetARRAY properties.
- InOut:
Scope
Name
Type
Comment
Return
GetBACnetArraySizeOfTwoPropertiesCmpBACnet.IEC_BACNET_STATUSInput
aePropertyIDsARRAY [0..2] OF CmpBACnet.IEC_BACNET_PROPERTY_ID
The ID of the property to get the array size from.
Output
arraySizeCmpBACnet.IEC_BACNET_ELEMENT_COUNT