BACnetObjectBase.GetBACnetAccumulatorRecordProperty (METH)

METHOD GetBACnetAccumulatorRecordProperty : CmpBACnet.IEC_BACNET_ACCUMULATOR_RECORD

Returns the BACnet-Accumulator-Record of the specified Property (propID) of this BACnet-Object as a IEC_BACNET_ACCUMULATOR_RECORD struct. The used functions are no client, meaning, that the access of the property is not restricted by write or read access restrictions.

InOut:

Scope

Name

Type

Comment

Return

GetBACnetAccumulatorRecordProperty

CmpBACnet.IEC_BACNET_ACCUMULATOR_RECORD

Input

propID

CmpBACnet.IEC_BACNET_PROPERTY_ID

The ID of the property to get.