BACnetStructuredView.GetSubordinateCount (METH)
METHOD GetSubordinateCount : CmpBACnet.IEC_BACNET_STATUS
Gets the number of subordinates and a subordinate anotations in the Subordinate_List-Property and the Subordinate_Annotations-Property of this BACnet-Object. Both the subordinate and its annotation have to have the same number of entries, so only one count is returned.
- InOut:
Scope
Name
Type
Comment
Return
GetSubordinateCountCmpBACnet.IEC_BACNET_STATUSOutput
countCmpBACnet.IEC_BACNET_ELEMENT_COUNTThe count of subordinates after the method call.