BACnetStructuredView.GetSubordinate (METH)
METHOD GetSubordinate : CmpBACnet.IEC_BACNET_STATUS
Gets a subordinate (given by a BACnet-Object-Reference) and a subordinate anotation at index nIndex from the Subordinate_List-Property and the Subordinate_Annotations-Property of this BACnet-Object. Both the subordinate and its annotation are aquired simulatenously by this function.
- InOut:
Scope
Name
Type
Comment
Return
GetSubordinateCmpBACnet.IEC_BACNET_STATUSInput
nIndexCmpBACnet.IEC_BACNET_ELEMENT_COUNTThe 1 based index of the subordnate to get.
Output
subordinateCmpBACnet.IEC_BACNET_DEV_OBJ_REFERENCEThe gotten subordnate reference after the method call.
annotationWSTRING(255)The annotation of the gotten subordinate after the method call.