BACnetStructuredView.AddSubordinate (METH)
METHOD AddSubordinate : CmpBACnet.IEC_BACNET_STATUS
Adds a subordinate (given by a BACnet-Object-Reference) and a subordinate anotation to the Subordinate_List-Property and the Subordinate_Annotations-Property of this BACnet-Object. Both the subordinate and its annotation are added simulatenously by this function.
- InOut:
Scope
Name
Type
Initial
Comment
Return
AddSubordinateCmpBACnet.IEC_BACNET_STATUSInput
deviceInstanceCmpBACnet.IEC_BACNET_DWORDThe device to reference by the subordinate
objInstanceCmpBACnet.IEC_BACNET_DWORDThe object instance number to reference by the subordinate.
objTypeCmpBACnet.IEC_BACNET_OBJECT_TYPEThe object type to reference by the subordiante.
xDevicePresentBOOLTRUE
Whether the device is present or not.
annotationWSTRING(255)The annotation (comment) for the subordinate added.