BACnetSchedule.GetExceptionEntry (METH)
METHOD GetExceptionEntry : CmpBACnet.IEC_BACNET_STATUS
Gets a entry with index nIndex of the Exception_Schedule-Property of this BACnet-Object. The returned data (pSpecialEvt) is allocated by the stack and therefore has to be freed after usage using FreeStackAllocatedMemory again!
- InOut:
Scope
Name
Type
Comment
Return
GetExceptionEntryCmpBACnet.IEC_BACNET_STATUSInput
nIndexCmpBACnet.IEC_BACNET_ELEMENT_COUNTThe 1 based index of the exception entry to get.
Output
pSpecialEvtPOINTER TO CmpBACnet.IEC_BACNET_SPECIAL_EVENT
The returned Pointer gets filled with the data of IEC_BACNET_EVENT_PARAMETER AND (!) the data referenced within evtParams. After usage, use FreeStackAllocatedMemory, to free the used memory again.