BACnetSchedule.AddExceptionBACnetDateRange (METH)
METHOD AddExceptionBACnetDateRange : CmpBACnet.IEC_BACNET_STATUS
Adds a date range to the Exception_Schedule-Property of this BACnet-Object.
- InOut:
Scope
Name
Type
Comment
Return
AddExceptionBACnetDateRangeCmpBACnet.IEC_BACNET_STATUSInput
bacStartDatCmpBACnet.IEC_BACNET_DATEThe start of the exception date range.
bacEndDatCmpBACnet.IEC_BACNET_DATEThe end of the exception date range.
pEntriesPOINTER TO CmpBACnet.IEC_BACNET_TIME_VALUE
The times and values during the date range which correspond to the exception date.
entryCountCmpBACnet.IEC_BACNET_ELEMENT_COUNTThe number of times and values for the exceptions.
eventPriorityBYTEThe priority with which the values are written.