BACnetSchedule.AddExceptionBACnetDate (METH)
METHOD AddExceptionBACnetDate : CmpBACnet.IEC_BACNET_STATUS
Adds a date to the Exception_Schedule-Property of this BACnet-Object.
- InOut:
Scope
Name
Type
Comment
Return
AddExceptionBACnetDateCmpBACnet.IEC_BACNET_STATUSInput
bacDatCmpBACnet.IEC_BACNET_DATEThe exception date to add.
pEntriesPOINTER TO CmpBACnet.IEC_BACNET_TIME_VALUE
The times and values during the date which correspond to the exception date.
entryCountCmpBACnet.IEC_BACNET_ELEMENT_COUNTThe number of times and values for the exceptions.
eventPriorityBYTEThe priority with which the values are written.