BACnetCommand.RemoveActionList (METH)

METHOD RemoveActionList : CmpBACnet.IEC_BACNET_STATUS

Removes a action list and action list text at index nIndex from the Action-BACnet-Propetrty and Action_Text-BACnetProperty of this BACnet-Command-Object at the same time. So both description and action are removed simultaneously.

InOut:

Scope

Name

Type

Comment

Return

RemoveActionList

CmpBACnet.IEC_BACNET_STATUS

Input

nIndex

CmpBACnet.IEC_BACNET_ELEMENT_COUNT

The 1 based index of the action list (and text) to remove.