BACnetCommand.AddActionList (METH)
METHOD AddActionList : CmpBACnet.IEC_BACNET_STATUS
Adds a action list and action list text to the Action-BACnet-Propetrty and Action_Text-BACnetProperty of this BACnet-Command-Object at the same time. So both description and action are added simultaneously (inputs actionList with corresponding description actionListText). The entries of the action list (actionList) may be initialized using the helper functions InitializeActionCommandBACnetBinaryPV,… of this FB.
- InOut:
Scope
Name
Type
Comment
Return
AddActionListCmpBACnet.IEC_BACNET_STATUSInput
actionListCmpBACnet.IEC_BACNET_ACTION_LISTThe action list to add to the Action-Property.
actionListTextWSTRING(255)The action text to add to the Action_Text-Property.