BACnetCommand.GetActionList (METH)
METHOD GetActionList : CmpBACnet.IEC_BACNET_STATUS
Gets a action list and action list text at index nIndex from the Action-BACnet-Propetrty and Action_Text-BACnetProperty of this BACnet-Command-Object at the same time. So both description and action are aquired simultaneously (outputs pActionList and sctionListText).
- InOut:
Scope
Name
Type
Comment
Return
GetActionListCmpBACnet.IEC_BACNET_STATUSInput
nIndexCmpBACnet.IEC_BACNET_ELEMENT_COUNTThe 1 based index of the action list to get.
Output
pActionListPOINTER TO CmpBACnet.IEC_BACNET_ACTION_LIST
The returned Pointer gets filled with the data of IEC_BACNET_EVENT_PARAMETER AND (!) the data referenced within evtParams. After usage, use FreeStackAllocatedMemory, to free the used memory. The pointer only points to a single action list.
actionListTextWSTRING(255)The corresponding action text describing the aquired action list.