EFilterLatchContent (ENUM)
TYPE EFilterLatchContent :
This enumeration describes how to interpret the value of filter by latch variable content
- Attributes:
qualified_only- InOut:
Name
Initial
Comment
NOT_SET
-1
Filter is not already set
DISABLE
0
Filter is disabled
STR
1
Variable for filtering contains a literal value: e.g. ‘ABCD’ ‘123’ “ABCD” “123”
IEC
2
Variable for filtering contains a string that has to be interpret as IEC notation number: e.g. t#2s
NUMBER
3
Variable for filtering contains a string that has to be interpret as number: e.g. “123”, “456.4”