EAlarmType (ENUM)

TYPE EAlarmType :

This enumeration is used to distinguish between alarms and events.

Attributes:
qualified_only
InOut:

Name

Initial

Comment

Undefined

0

Undefined, resp. represents the absence of a value

Alarm

1

An alarm.

Event

2

An event, that must be acknowledged by the user (has acknoledge method ACK)

ImplicitlyAcknowledgedEvent

3

An event with acknowledge method REP, that is implicitly acknowledged and only written into the alarm storage (not visible in the list of active alarms).