AUTOTUNE_ERROR_ID (ENUM)

TYPE AUTOTUNE_ERROR_ID(

NO_ERROR

Enumeration of the Autotune Error ID, describes the details of each error generated by function block when auto tune fault occurs

Attributes:
qualified_only
InOut:

Name

Initial

Comment

NO_ERROR

16#0

1: No Error

STEP_CHANGE_SMALL

16#72C0

2: The step change (Sp-Pv) was too small when adaption was started, a value of 120*Range/ Resolution is required as a minimum change.Resolution: 4096, Range: tsMachineSet.rTcMax * tsInternalStatus.iRawFactor.

INSUFFICIENT_MEASUREMENT_INTERVALS

16#72C1

3: Not enough measured points to calculate the tangent => increase the step change/decrease the scan time

DELAY_TIME_SMALL

16#72C2

4: Delay time could not be measured, probably too small

ADAPTION_LONG

16#72C3

5: Adaption needs too long (any time measured >32700 => increase the scan time/increase the value for CvAdapt .