SolarNormalizeAnalog (FUN)
FUNCTION SolarNormalizeAnalog : REAL
Function to integrate is used to easily integrate, with any S500 AI/AO card, standard sensor type 4-20 mA or 0-10V as positioning sensors for Solar Trackers. This function can be used to integrate analog sensors such as inclinometers
According to the signal sensor provided and the movement range of the system, SolarNormalizeAnalog gets the current system position. Internally function SolarNormalizeAnalog uses the corresponding decimal values given by the AI/AO card when an analog input is detected
- InOut:
Scope
Name
Type
Initial
Comment
Return
SolarNormalizeAnalogREALInput
EnableBOOLFALSE
1: Enable function by TRUE level at the input.
LevLowREAL0
2: The lower limit of the movement range in Degrees.
LevHighREAL0
3: The upper limit of the movement range in Degrees.
InputSignalREAL0
4: Input Analog sensor signal.