SolarNSAxisSecondary (FUN)
FUNCTION SolarNSAxisSecondary : LREAL
This function provides the angle of secondary axis for solar tracking, in two axes, according to: elevation, azimuth, correction alignment factor and angle of main axis.
This function assumes the East to West axis as the main system axis. This function is valid when east to west axis is acting as the main axis
Alignement correction is the angle between system axis and east (clockwise)
EWAxisPrim provides the Angle of main axis (0°=zenith, -90°=north, 90°=south) like explained in below image,
The block output is the angle of secondary axis north to south, where zenith indicates 0° position. Output value is in Degrees with range -180.00…180.00. Negative value indicates clockwise rotation about north to south axis. Otherwise, positive value indicates anticlockwise rotation about the north to south axis.
- InOut:
Scope
Name
Type
Initial
Comment
Return
SolarNSAxisSecondaryLREALInput
AzimuthLREAL0
1: Topocentric azimuth angle. Eastward from north (0°=360°=north, 90°=east, 180°=south, 270°=west). Format: Degrees, Range: 0 to 359.9999
ElevationLREAL0
2: Topocentric elevation angle (0°=sunrise, 90°=zenith). Format: Degrees, Range: -90.00…90.00. Negative values = darkness
AlignmentCorrectionLREAL0
3: Angle between system axis and north (clockwise). Format: Degrees, Range: -180.00…180.00.
EWAxisPrimLREAL0
4: Angle of main axis (0°=zenith, -90°=north, 90°=south). Format: Degrees.