ModTcpServOnOff (FB)

FUNCTION_BLOCK ModTcpServOnOff EXTENDS AbbETrig3

Function Block serves to set Modbus TCP server to active/passive

InOut:

Scope

Name

Type

Initial

Comment

Inherited from

Input

Execute

BOOL

FALSE

A rising edge starts a single operation, the output Busy goes to TRUE. In the first cycle all other inputs are read and stored, afterwards they are ignored. A falling edge does not stop the operation. After Done = TRUE or Error = TRUE and Execute = FALSE all outputs will be reset. For executing another operation the Execute input needs to be retriggered by another rising edge!

AbbETrig3

Output

Done

BOOL

FALSE

Operation is completed without error (while outputs Busy and Error are FALSE). This output is TRUE for at least one cycle or until Execute is set to FALSE

AbbETrig3

Busy

BOOL

FALSE

Operation is running (while outputs Done and Error are FALSE)

AbbETrig3

Error

BOOL

FALSE

Operation is stopped with error (while outputs Busy and Done are FALSE). This output is TRUE for at least one cycle or until Execute is set to FALSE. The output ErrorID gives more details about the error.

AbbETrig3

Input

Eth

BYTE

ETH1

Index number of the assigned interface

On

BOOL

TRUE

Switch on (TRUE) or off (FALSE) server

Output

ErrorID

ERROR_ID

ERROR_ID.NO_ERROR

Error code describing error condition
NO_ERROR - Execution successfully completed
ERR_INVALID_INTERFACE - Invalid Ethernet interface or no Server configured on Ethernet interface
ERR_ALREADY_IN_STATE - Server already in requested state
ERR_SIMULTANEOUS_ACCESS - Server already accessed by other FB instance, try again later on
ERR_FAILED_SET_STATE - Failed to set Server to requested state
ERR_INTERNAL_UNEXPECTED_STATE - Unexpected state. Fatal internal error
ERR_UNKNOWN - Undefined error