ModTcpConfig (FB)

FUNCTION_BLOCK ModTcpConfig EXTENDS AbbETrig3

Configuration Modbus TCP

InOut:

Scope

Name

Type

Initial

Comment

Inherited from

Input

Execute

BOOL

FALSE

A rising edge starts a single operation, the output Busy goes to TRUE. In the first cycle all other inputs are read and stored, afterwards they are ignored. A falling edge does not stop the operation. After Done = TRUE or Error = TRUE and Execute = FALSE all outputs will be reset. For executing another operation the Execute input needs to be retriggered by another rising edge!

AbbETrig3

Output

Done

BOOL

FALSE

Operation is completed without error (while outputs Busy and Error are FALSE). This output is TRUE for at least one cycle or until Execute is set to FALSE

AbbETrig3

Busy

BOOL

FALSE

Operation is running (while outputs Done and Error are FALSE)

AbbETrig3

Error

BOOL

FALSE

Operation is stopped with error (while outputs Busy and Done are FALSE). This output is TRUE for at least one cycle or until Execute is set to FALSE. The output ErrorID gives more details about the error.

AbbETrig3

Input

RespTimeout

WORD

DEFAULTS.CONFIG_RESPONSE_TIME

Slave response timeout in ms. Maximum time waiting for a response after having sent a request

KeepAlive

DWORD

DEFAULTS.CONFIG_KEEP_ALIVE

Open Modbus Time in ms. A connection to a Server stays open after sending a request

until the time is expired. If there is another request within this time, the timer is restarted. On expiration the connection is closed.

ByteOrder

CAA.ENDIANESS

DEFAULTS.CONFIG_BYTE_ORDER

Endianess of data, little or Big Endian; Modbus Standard is Big Endian

Port

WORD

DEFAULTS.CONFIG_PORT

TCP Port

Output

ErrorID

ERROR_ID

ERROR_ID.NO_ERROR

Error code describing error condition
NO_ERROR - Execution successfully completed
ERR_ENDIANESS_NOT_SUPPORTED - Endianess / byte order not supported
ERR_UNKNOWN - Undefined error