OBIOMotionSinglePTO (FB)

FUNCTION_BLOCK OBIOMotionSinglePTO EXTENDS AbbLConC3

Single axis point-to-point or velocity movement, utilizing the PTO functionality for AC500 eco CPU.

precondition

the respective channel is configured as PTO channel.

Up to 4 single PTO channel are possible. The max possible frequency is 200kHz.
basic input parameters

OpenLoop

TRUE: There is no external position feedback available. The pulses output are used as actual position.
FALSE: A position feedback is used. The actual position has to be written to ActPosition.
MaxFrequency

Used as a reference Value to calculate the acceleration and deceleration. The axis will run from MinFrequency to MaxFrequency in RefAcceleration[ms] time.

MinFrequency

The movement will start and end with MinFrequency. The Value should not be too small: 1Hz would mean the first/last step needs 1s.

Cycle

cycle time for the PLC program [ms]. A wrong setting for “Cycle” will result in wrong acceleration/deceleration ramps

p2p

provides the positioning method. It can either be of type OBIOBasicPoint2Point, which will use trapezoidal ramps, or of type OBIOSineSquaePoint2Point, which will use sinesquare ramps.


velocity movement

  • A continuous velocity movement is started with a rising edge at ExecuteVel.

  • The parameters used are RefFrequency, RefDirection, RefAcceleration and RefDeceleration.

  • These paremeters can be changed during the movement and will be used immediately.

  • The output InVelocity indicates that the required velocity is reached.

  • The movement can be stopped with input Stop.

positioning movement

  • A positioning movement can be started with a rising edge at ExecutePos. It is an absolute positioning.

  • The parameters used are RefFrequency, RefAcceleration, RefDeceleration and RefPosition. No new values will be accepted during the movement.

  • The output InPosition indicates that the movement is completed.

  • The movement can be stopped with input Stop.

Note

This block should just be called once per cycle otherwise inconsistent values could be send to PRU, if send twice in short time.

InOut:

Scope

Name

Type

Initial

Comment

Inherited from

Input

Enable

BOOL

FALSE

A rising edge (Enable = TRUE) starts the operation, the output Busy goes to TRUE. All other inputs are read and considered continuously. Execution will continue forever until a falling edge (Enable = FALSE) aborts the operation. During Aborting the Busy is still TRUE. Afterward all outputs are reset.

AbbLConC3

Output

Busy

BOOL

FALSE

Operation is running (while output Error is FALSE)

AbbLConC3

Error

BOOL

FALSE

Operation is stopped with error (while output Busy is FALSE). This output is TRUE for at least one cycle or until Enable is set to FALSE. The output ErrorID gives more details about the error.

AbbLConC3

Input

Channel

BYTE

single PTO channel, 0..3, requires according configuration

OpenLoop

BOOL

TRUE

do not use the ActPosition as input if OpenLoop=TRUE is set. Instead, the number of pulses send to PTO output will be written on ActPosition

ResetPos

BOOL

Reset the position on rising edge to “0”, just allowed when Busy=FALSE

ExecutePos

BOOL

start the algorithm with a rising edge, absolute positioning, just allowed with Busy=FALSE

ExecuteVel

BOOL

start a continuous movement with a rising edge,just allowed with Busy=FALSE

Stop

BOOL

Stop using RefDeceleration. Stop will overrule ExecutePos and ExecuteVel

RefPosition

DINT

absolute position, where to move with rising edge at ExecutePos

RefFrequency

DWORD

Reference Frequency in Hz, can be continuously changed for velocity movement

RefDirection

BOOL

direction, used for velocity movement

RefAcceleration

TIME

TIME#1s0ms

Acceleration as time in ms to run from MinFrequency to MaxFrequency

RefDeceleration

TIME

TIME#1s0ms

Deceleration as time in ms to run from MinFrequency to MaxFrequency

MaxFrequency

DWORD

200000

maximum frequency for frequency output, new value just used with Enable=FALSE

MinFrequency

DWORD

500

minimum for frequency output, new value just used with Enable=FALSE

Cycle

INT

1

Cycle time of the PLC-Program in ms, new value just used with Enable=FALSE

EncoderScaling

LREAL

1

EncoderScaling, can be used with OpenLoop=FALSE, is ignored otherwise. The parameter will just modify the positioning movement.
  • Usage: the encoder might have a different number of increments per revolution, compared to the stepper motor.

  • for example:

  • motor = 1000 inc/r, encoder = 1000 inc/r *4 (4-fold counting) => EncoderScaling=4

  • motor = 1000 inc/r, encoder = 1024 inc/r => EncoderScaling=1.024

If this parameter has a wrong value, the deceleration ramp will not match the given parameter (in positioning movement), as it is adjusted to meet the RefPosition

Note

RefFrequency is issued as a frequency for the stepper motor, it is not affected by this parameter.

Note

a higher position resolution (encoder with more increments) will result in shorter positioning time, with otherwise not modifed parameters.

InterpolationType

OBIOInterpolationType

Decide if trapezoidal or sinesquare ramp for positioning is to be used

Inout

ActPosition

DINT

Actual position

Output

ErrorID

Error_ID

Error Code

Active

BOOL

positioning is completed A new movement can just be started with Active=FALSE. Active is mutually exclusive with InPosition. A ExecutePos for the current position might result in InPosition without showing Active.

InPosition

BOOL

positioning is completed

InVelocity

BOOL

RefFrequency=ActFrequency

ActFrequency

DWORD

moving frequency for the drive in inc/s. This value is send to the PTO channel (FB (INTERNAL)).

ActDirection

BOOL

TRUE means: move forward. This value has to be connected to a binary output.