DrvPnRead (FB)

FUNCTION_BLOCK DrvPnRead EXTENDS AbbETrig3

Function block DrvPnRead reads maximum 37 parameters from the drive in a single DPV1 query. The number of parameters to be read is specified at the input Nvar.

Parameters to read from the drive are specified at the Data input. DrvPbPnPrmDpv1DataType structure must be declared to a variable and connected to Data input using ADR. This structure contains the Group, Index, which must be given to the variable. Read parameter type and values are stored in the same variable

DrvPdPrmDpv1DataType structure has the following array elements

  • abyPrmGroup: Array of 37 WORD for specifying parameter Group.

  • abyPrmIndex: Array of 37 WORD for specifying parameter Index.

  • abyPrmType: Array of 37 DRV_PDRIVE_PRM_TYPE. Read parameter data type will be available here. For details refer to DRV_PDRIVE_PRM_TYPE. If a type is set here at the start, it can be compared with the type value read from the drive if the Compare input is set.

  • adwPrmValue: Array of 37 DWORD. Read parameter value will be available here. If a value is set at the start, it can be compared with the value read from the drive if the Compare input is set.

Read errors

If the drive rejects to read a specific parameter, it returns the error code DRV_ERROR_PRM (16#44) in the corresponding abyPrmType element and a more specific error value in the corresponding adwPrmValue element.

The number of elements with errors from the drive are given at the output “NumPrmErrors”. The output “PrmErrCmpValues” gives an array, which contains the more specific error values in the elements (index). This can be used to quickly identify the errorneous elements.

Compare input

As the DrvPnWrite function block does not return an error in case a parameter in the drive could not be written correctly it is recommended to verify the writing. This can be done with the call of this function block DrvPnRead if the same parameters, types and values are connected to the Data input (use the same struct as for the writing), and the input “Compare” is set to TRUE.

Then the types and values of the connected struct are copied at the rising edge of Excecute inputs and compared with the returned types and values from the drive. In case of a diffrence this is set into the corresponding element of the output array PrmErrCmpValues with the possible three error codes DRV_CMP_DIFF_TYPE, DRV_CMP_DIFF_VALUE or DRV_CMP_DIFF_TYPE_AND_VALUE.

Mode input

  • Mode = 16#00 => Read direct variables and parameters via an Fxxx module, e.g. FENA-21 or FPNO-21. Group and Index have to be used as in the Data.awPrmGroup and Data.awPrmIndex array. (Number of Elements in the PN Datablock is set to 16#01)

  • Mode = 16#01 => Read direct variables and parameters via an Rxxx module, e.g. RETA-02 for ACS800 or DCS500. Group and Index have to be used as in the Data.awPrmGroup and Data.awPrmIndex array. (Number of Elements in the PN Datablock is set to 16#01)

  • Mode = 16#1x => to be used to access PROFIDrive parameters with Attribute = 16#10 (Value) and Number of Elements = x.

  • Mode = 16#2x => to be used to access PROFIDrive parameters with Attribute = 16#20 (Description) and Number of Elements = x. (Not supported with Fxxx or Rxxx modules)

  • Mode = 16#3x => to be used to access PROFIDrive parameters with Attribute = 16#30 (Text) and Number of Elements = x. (Not supported with Fxxx or Rxxx modules)

For PROFIDrive parameters using Mode = 16#1x, 16#2x or 16#3x the Number of Elements = x is used for all the parameters in the Data array.

Note

If multiple DrvPnRead and /or multiple DrvPnWrite Functions Blocks for the same device are enabled at the same time, it may cause a Read/ Write error.

InOut:

Scope

Name

Type

Initial

Comment

Inherited from

Input

Execute

BOOL

FALSE

A rising edge starts a single operation, the output Busy goes to TRUE. In the first cycle all other inputs are read and stored, afterwards they are ignored. A falling edge does not stop the operation. After Done = TRUE or Error = TRUE and Execute = FALSE all outputs will be reset. For executing another operation the Execute input needs to be retriggered by another rising edge!

AbbETrig3

Output

Done

BOOL

FALSE

Operation is completed without error (while outputs Busy and Error are FALSE). This output is TRUE for at least one cycle or until Execute is set to FALSE

AbbETrig3

Busy

BOOL

FALSE

Operation is running (while outputs Done and Error are FALSE)

AbbETrig3

Error

BOOL

FALSE

Operation is stopped with error (while outputs Busy and Done are FALSE). This output is TRUE for at least one cycle or until Execute is set to FALSE. The output ErrorID gives more details about the error.

AbbETrig3

Input

CmDevice

AC500_DeviceBase.IRoleProfinetController

2: Name of the Communication Module Device connected, Example: CM579_PNIO or CM579_PNIO_1 or Profinet_IO_Controller

DevName

STRING(INT#240)

3: Profinet Name of the device (drive), Example: ‘abbdrive-38’

DevSlot

UINT

1

4: Device Slot from which the data object is to be read - For all ACS/DCS Drives “1” should be used.

DevSubSlot

UINT

1

5: Device SubSlot from which the data object is to be read - For all ACS/DCS Drives “1” should be used.

Mode

BYTE

0

6: Mode = 0: Fxxx- modules e.g. FENA-21 or FPNO-21. Mode = 1: Rxxx modules used e.g. RETA-02 (ACS800, ACS500); Other modes for Profidrive parameters see description.

MaxRetries

BYTE

4

7: Maximum numbers of retries of internal read / write telegrams if device responses with “state conflict”. Maximum: 10.

WaitTimeRetry

WORD

200

8: Waiting time [ms] before a new retry is started after response with “state confict”. 0 = Automatic calculation according to actual data size; Min: 40ms; Max: 2000ms;

Compare

BOOL

FALSE

9: Compare is performed with “abyPrmType” and “abyPrmValue” elements. Can be used to verify the before written data.

Nvar

BYTE

10: Number of parameters to read

Data

DWORD

11: Address of variable of “DrvPdPrmDpv1DataType”. Connect via ADR operator. For Parameter Group, Index, Type and Value

Output

ErrorID

ERROR_ID

ERROR_ID.NO_ERROR

4: Error codes

AddErrorID1

AC500_CM579Profinet.ERROR_ID

AC500_CM579Profinet.ERROR_ID.NO_ERROR

5: Error ID from internal called ProfinetCommonRead or ProfinetCommonWrite block.

AddErrorID2

UDINT

0

6: AddErrNo output number from internally called PnioCtrlRead or PnioCtrlWrite block. See library AC500_CM579Profinet.

Status

DWORD

0

7: Status output from internal called PnioCtrlRead or PnioCtrlWrite block - see Profidrive description in fieldbus module manual or AC500-V2 docu “Profinet Status” in Profinet IO library. (E.g. 16#DF80B500 = Write Response State conflict. –> Try to increase MaxRetries or WaitTimeRetry)

AddVal1

WORD

0

8: Additional Value 1 - AddVal1 output from internally called PnioCtrlRead or PnioCtrlWrite block see library AC500_CM579Profinet

AddVal2

WORD

0

9: Additional Value 2 - AddVal2 output from internally called PnioCtrlRead or PnioCtrlWrite block see library AC500_CM579Profinet

DataLen

UINT

0

10: Package size of the Read response. DataLen output from the internal Read block PnioCtrlRead

NumPrmErrors

BYTE

0

11: Number of parameters that could not be read. Check abyPrmType for 16#44 (DRV_ERROR_PRM) then the abyPrmValue represents the error code.

NumPrmCmpDiff

BYTE

0

12: Number of parameters that showed diffrences in either type or value at Compare. Check PrmErrorValues[] for DRV_CMP_DIFF_TYPE, DRV_CMP_DIFF_VALUE or DRV_CMP_DIFF_TYPE_AND_VALUE.

PrmErrCmpValues

ARRAY [1..37] OF DRV_PDRIVE_PRM_REQ_ERROR

[37(DRV_NOT_USED)]

13: Error values and compare differences per parameter index

Methods:

A_StartAction

B_CyclicAction

C_CleaningAction

D_ResetAction

Structure: