IoProdEntryRead (FB)
FUNCTION_BLOCK IoProdEntryRead EXTENDS AbbETrig
Read production data out of the I/O - Modules with Firmware >= V3.0
- InOut:
Scope
Name
Type
Initial
Comment
Inherited from
Input
ExecuteBOOLFALSE
A rising edge starts the operation, the output Busy goes to TRUE. In the first cycle all other inputs are read and stored, afterwards they are ignored. A falling edge does not stop the operation. After Done = TRUE or Error = TRUE and Execute = FALSE all outputs will be reset.
AbbETrig
Output
DoneBOOLFALSE
Operation is completed without error (while outputs Busy and Error are FALSE). This output is TRUE for at least one cycle or until Execute is set to FALSE
AbbETrig
BusyBOOLFALSE
Operation is running (while outputs Done and Error are FALSE)
AbbETrig
ErrorBOOLFALSE
Operation is stopped with error (while outputs Busy and Done are FALSE). This output is TRUE for at least one cycle or until Execute is set to FALSE. The output ErrorID gives more details about the error.
AbbETrig
Input
ModuleBYTE1
Module number 1…10
Output
ErrorIDERROR_ID.NO_ERROR
Error code describing error condition
IdentNumSTRING(15)‘’
Ident number of the IO-module
IndexNumSTRING(2)‘’
Index of the IO-module
IOTypeSTRING(14)‘’
Type of the IO-module
ManufactWeekSTRING(2)‘’
Manufactory week of the IO-module
ManufactYearSTRING(2)‘’
Manufactory year of the IO-module
BAInstSTRING(5)‘’
Ba inst of the IO-module
FactoryIdSTRING(2)‘’
Manufactory place of the IO-module
SerialNumSTRING(8)‘’
Serial number of the IO-module