'Project' 'Rebuild all'Permalink

With 'Project' 'Rebuild all', unlike the incremental compilation, the project is completely recompiled. Download information is not discarded, however, as is the case with the command 'Project' 'Clean all'. Note the possibility to exclude objects from compilation.

⮫ “'Project' 'Build'”

⮫ “'Project' 'Clean all'”

⮫ “'Project' 'Load download information'”

⮫ “Options for build”

See 'Online' 'Login' for a diagram showing the relations between Project-Build, Project-Download, Online Change and Login on the target system.

Figure