OverviewPermalink

You can use the following commands in all editors and some of them in the Object Organizer. The commands are located under the menu item 'Edit' and in the context menu that is opened with the right mouse button.

If the IntelliPoint-Software is installed on the computer, all functions of the MS IntelliMouse are supported. In all editors with zoom functionality: To magnify press the <Strg> key while rolling the wheel of the mouse, to reduce roll backwards while the <Ctrl> key is pressed.

⮫ “'Edit' 'Undo'”

⮫ “'Edit' 'Redo'”

⮫ “'Edit' 'Cut'”

⮫ “'Edit' 'Copy'”

⮫ “'Edit' 'Paste'”

⮫ “'Edit' 'Delete'”

⮫ “'Edit' 'Find'”

⮫ “'Edit' 'Find next'”

⮫ “'Edit' 'Replace'”

⮫ “'Edit' 'Input assistant'”

⮫ “Unstructured display”

⮫ “Structured display”

⮫ “'Edit' 'Autodeclare'”

⮫ “'Edit' 'Next error'”

⮫ “'Edit' 'Previous error'”

⮫ “'Edit' 'Macros'”