'Edit' 'Cut'Permalink

symbol_bearb_ausschn (AC500-S PT)

Shortcut: <Ctrl>+<X> or <Shift>+<Delete>

This command transfers the current selection from the editor to the clipboard. The selection is removed from the editor.

In the 'Object Organizer' this similarly applies to the selected object, whereby not all objects can be deleted, e.g. the PLC Configuration.

⮫ “Object organizer”

⮫ “'Edit' 'Replace'”

Remember that not all editors support the cut command, and that its use can be limited in some editors.

The form of the selection depends upon the respective editor:

In the text editor ST, and declarations the selection is a list of characters.

In the FBD and LD editors the choice is a number of networks which are indicated by a dotted rectangle in the network number field or a box with all preceding lines, boxes, and operands.

In order to paste the content of the clipboard you use the command 'Edit' 'Paste'.

⮫ “'Edit' 'Paste'”

In order to remove a selected area without changing the clipboard, use the command 'Edit' 'Delete'.

⮫ “'Edit' 'Delete'”