You can configure settings that affect the behavior of CODESYS and that of certain editors in the “Project Settings” object. The settings are valid throughout the project and are applied immediately for active editors. You can also access the dialog boxes of the object with the command “Project Project Settings”.
CODESYS saves the project settings as an object directly in the project. If you then transfer a project to another system, the “Project Settings” object is also transferred with it, without a project archive being required.
See also