Symbol: 
Function: This dialog activates the tests that the light version of CODESYS Static Analysis performs each time code is generated.
Call: Menu bar: “Project Project Settings” (“Static Analysis Light” category).
You can exclude lines of code from the static code analysis by marking the code with
the pragma {analysis ...} or the pragma {attribute 'analysis' := '...'}.
Additional compile tests
|
“SA0033: Unused variables” |
Finds variables that are declared, but not used within the compiled program code. For GVL variables: If there are multiple applications in one project, then only the
objects under the currently active application are affected. If there is only one
application, then the objects in the |
|
“SA0028: Overlapping memory areas” |
Detects the locations where two or more variables reserve the same storage space.
For example, this occurs for the following declarations: |
|
“SA0006: Write access from multiple tasks” |
Detects variables that are written by more than one task. |
|
SA0004 “Multiple write access on output” |
Detects outputs that are written to more than one location. Note: No error is reported when an output variable ( Note: A pragma cannot deactivate this rule. |
|
“SA0027: Multiple use of identifiers” |
Detects multiple uses of a name/identifier for a variable or an object (POU) within the scope of a project. The following cases are detected:
|
|
“SA0167: Temporary function block instances” |
The test detects function block instances that are declared as temporary variables.
This concerns instances that are declared in a method or in a function or as |
Examples
SA0003: Empty statements
; (* Comment *); iVar;
SA0006: Concurrent access
FUNCTION_BLOCK ADD_FB g_iTemp1 := g_iTemp1 + INT#1;
PROGRAM PLC_PRG //controlled by MainTask g_iTemp1 := g_iTemp1 + INT#2; g_xTemp2 := g_iTemp1 > INT#10;
PROGRAM PLC_PRG_1 //controlled by SubTask g_iTemp1 := g_iTemp1 - INT#3; g_xTemp2 := g_iTemp1 < INT#-10;
SA0004 Multiple write access on output
VAR_GLOBAL
g_xVar AT %QX0.0 : BOOL ;
g_iTest AT %QW0 : INT ;
END_VAR
PROGRAM PLC_PRG
IF iCondition < INT#0 THEN
g_xVar := TRUE;
g_iTest := INT#12;
END_IF
CASE iCondition OF
INT#1:
g_xVar := FALSE;
INT#2:
g_iTest := INT#11;
ELSE
g_xVar := TRUE;
g_iTest := INT#9;
END_CASE
SA0006: Write access from multiple tasks
FUNCTION_BLOCK ADD_FB g_iTemp1 := g_iTemp1 + INT#1; PROGRAM PLC_PRG // Controlled by MainTask g_iTemp1 := g_iTemp1 + INT#2; g_xTemp2 := g_iTemp1 > INT#10; PROGRAM PLC_PRG_1 //Controlled by SubTask g_iTemp1 := g_iTemp1 - INT#3; g_xTemp2 := g_iTemp1 < INT#-10;
SA0027: Multiple use of name
PROGRAM PLC_PRG VAR ton : INT; // error SA0027 END_VAR
SA0029: Different notation in implementation and declaration
The PLC_PRG POU and a fnc function POU are in the device tree.
PROGRAM PLC_PRG VAR iVar:INT; _123test_var_: INT; END_VAR ivar := iVar + 1; // notation different to that in the declaration part -> SA0029 _123TEST_var_ := _123test_var_INT; // notation different to that in the declaration part -> SA0029 Fnc(); // notation different to that in the devices tree -> SA0029 END_VAR
SA0167: Temporary function block instances
PROGRAM PLC_PRG
VAR
END_VAR
VAR_TEMP
yafb: AFB;
END_VAR
FUNCTION Fun : INT
VAR_INPUT
END_VAR
VAR
funafb: AFB;
END_VAR
METHOD METH: INT
VAR_INPUT
END_VAR
VAR
methafb: AFB;
END_VAR
See also