Symbol: 
Function: The dialog is used to configure the project-wide settings for objects of type “Visualization”.
Call: Menu bar: “Project Project Settings”, “Visualization” category
Requirement: A project is open.
Tab 'General'
|
“Text list files” |
Directory which contains text lists that are available in the project to configure texts for different languages. CODESYS uses the directory, for example to import or export text lists. After clicking |
|
“Image files” |
Directory which contains image files that are available in the project. Multiple folders are separated with a semicolon. CODESYS uses the directory, for example to import or export image files. After clicking |
|
“Activate property handling in all element properties” |
Requirement: Its IEC code contains at least an object of type “Interface property” (a property ![]() Requirement: “Visible” is selected. |
|
“Enable implicit checks for visualization POUs” |
|
See also
Tab 'Symbol Libraries'
|
“Symbol libraries” |
List of all installed symbol libraries (example: |
|
“Assigned” |
|
, the
: You can also configure a visualization element with a property
in those of its properties in which you select an IEC variable. Then 
: Symbol library is installed in the library repository, but