Tab 'Storage'
The recipe manager provides functions for maintaining user-defined variable lists, known as recipe definitions. The recipe definitions can be stored in recipe files on the PLC.
|
“Storage Type” |
“Textual”: CODESYS saves the recipe in a readable Format with the configured columns and delimiters. “Binary”: CODESYS saves the recipe in a non-readable binary format. This format requires less storage space. Note: You can read binary recipes again only if you have not changed the variable lists. |
|
“File path” |
Example: Path on the runtime system Notes:
Example of the file path in the runtime system: CODESYS saves a file in this directory for each recipe when downloading to the PLC. The requirement is that you select the “Recipe management in the PLC” option. The files are loaded to the recipe manager each time the application is restarted. |
|
“File extension” |
File extension for the recipe file in the format The resulting default name for recipe files is in the form |
|
“Separator” |
Delimiters between the individual values in the saved file |
|
“Available Columns” “ Selected Columns” |
Defines the information that is saved and in which order in the recipe file |
|
“Save as Default” |
CODESYS uses the settings on the tab throughout the entire project for all other recipe managers. |
Tab 'General'
|
“Recipe management in the PLC” |
|
|
“Save recipe changes to recipe files automatically” |
When “Recipe management in the PLC” is selected, there is the following option for saving the recipe:
|
|
When “Recipe management in the PLC” is selected, there are the following two options for downloading from the PLC: |
|
|
“Download only for exact match of the variable list” |
|
|
“Download variables with matching names” |
In this way, recipe files can also be downloaded if variables in the file or in the recipe definition have been deleted. |
|
“Overwrite existing recipes on download” |
Requirement: The “Storage Type” is “Textual” and the “Save recipe changes to recipe files automatically” option is selected. |
|
The following options are available for writing recipe values to the variables on the PLC: |
|
|
“Limit the variable to min/max when recipe value is out of the range” |
|
|
“Do not write to a variable when the recipe value is out of the min/max range” |
|
|
The following option is available for reading recipe values from the PLC into the recipe in the project: |
|
|
“Check recipe for changes” |
Always use the function block
The option can be used in order to update the recipe file in the local file system only if recipe values have changed on the PLC. However, it affects performance because it generates additional code for checking.
Note: As the file system is written to each call, the controller can be very burdened. |
Recipes during online mode
|
Menu commands |
Behavior of the recipes defined in the project |
Behavior of the defined recipes at runtime |
|---|---|---|
|
“Online Reset Warm” “Online Reset Cold” “Online Download” |
The recipes of all recipe definitions are downloaded with the values from the current projects. |
Dynamically generated recipes remain unchanged. |
|
“Online Reset Origin” |
The application is removed from the PLC. If a download is done again afterwards, then the recipes are restored as for an online reset warm. |
|
|
Shutdown and restart of the PLC |
After a restart, the recipes are downloaded again from the automatically created files. This will restore the same state as before shutdown. |
|
|
“Online Online Change” |
The recipe values remain unchanged. In runtime mode, a recipe can be changed only
via the function block command |
|
|
“Debug Stop” “Debug Start” |
The recipes remain unchanged when the PLC is stopped or started. |
|
|
Actions |
Recipes defined in the project |
Recipes defined at runtime |
|---|---|---|
|
“Online Reset Warm” “Online Reset Cold” “Online Download” |
The recipes of all recipe definitions are downloaded with the values from the current projects. However, these are set in the memory only. To save recipes to a file, you have to run the “Save Recipe” command explicitly. |
Dynamically generated recipes are lost. |
|
“Online Reset Origin” |
The application is removed from the PLC. When a download is performed afterwards, the recipes are restored. |
Dynamically generated recipes are lost. |
|
Shutdown and restart of the PLC |
After the restart, the recipes are downloaded again from the automatically created files. This will restore the same state as before shutdown. |
|
|
“Online Online Change” |
The recipe values remain unchanged. In runtime mode, a recipe can be changed only
via the function block command |
|
|
“Debug Stop” “Debug Start” |
The recipes remain unchanged when the PLC is stopped or started. |
|
button.
: Has to be selected for the user program or visualization elements to load recipes
at runtime. If you transfer recipes to the PLC exclusively via the
: The recipe is only downloaded if the file on the PLC contains all variables from
the variable list of the recipe definition of the application and these are sorted
in the same order. Additional entries at the end are ignored. If the required match
does not exist, then the error status
: With each method call, the current PLC variable values are first read into the recipe.
Then the recipe is written to the recipe file in the local file system.