In the recipe definition (1), you define different data sets for the variables, which are termed recipes (2).
You can toggle the display of the recipe definition between the flat list view (3) and the structured view (4). In the structured view, CODESYS groups variables according to structure.

|
“Type” |
Entered automatically |
|
“Name” |
Optional |
|
“Minimal Value” “Maximal Value” |
If the variable value is less than the “Minimal Value” or greater than the “Maximal Value”, then CODESYS sets the value to the “Minimal Value” or “Maximal Value”. |
|
“Comment” |
Additional information, for example the unit of the value. |
|
“Current Value” |
Current variable value; not shown in online mode |
|
“Add Sibling” |
Adds a sibling variable to the recipe definition. |
|
“Add Child” |
Adds a child variable to the recipe definition. |
See also