Symbol: 
Function: This command reads the variable values of a recipe from the controller and saves them to a file.
Call: Main menu “Recipes”.
Requirement: The application is in online mode and you have selected the value of a recipe in the recipe definition.
After choosing the command, you are prompted either to read the variable values to the recipe or only to save them. Updating the values in the recipe could require an online change when logging in again.
The values are saved with the default name for recipe files according to the settings for the recipe manager (tab “Storage”).