Symbol:
A “DeviceTrace” object shows trace data in one or more diagrams, as does a “Trace” object.
The difference is that a “DeviceTrace” directly accesses traces that are running on the controller. The object is inserted below the device in the device tree. Therefore there is no immediate dependency on the applications in the CODESYS project.
You can use the DeviceTrace for visualizing the processor load of a multicore controller.
For more information about the editor and its operation, refer to the help page for the “Trace” object.