Function: With this dialog, you define the structure and contents of the user interface.
Call: Main menu “Tools Customize” (“Menu”).
When you click “OK” to close the dialog, the changes are visible in the menu bar of the CODESYS user interface.
|
Display of currently defined menus, submenus, and included commands. In CODESYS, a menu or submenu caption is identified by the caption symbol ( |
|
|
“Add Command” |
Enabled when a command is selected. Adds a command above the selected command. Opens the “Add Command” dialog. Use the “Add Command” dialog for selecting one or more commands. Left part: List of categories. Right part: List of commands in the selected category. |
|
“Add Separator” |
Adds a separator above the selected command. |
|
“Add Popup Menu” |
Adds a popup menu above the selected menu, submenu, or command. Opens the “Add Popup Menu” dialog. |
|
“Edit Popup Menu” |
Opens the “Edit Popup Menu” dialog. |
|
“Reset” |
Resets the default settings of the entire menu. |
|
“Load” |
Loads the settings from a stored file (<file name>.opt.menu). |
|
In CODESYS, a new menu is shown in the menu bar only when the menu contains at least one command. |
|
|
“Default text” |
Select this check box when localization is available. |
|
“Localized Texts” |
List: Languages and localized texts. |
|
“Add Language” |
Opens a drop-down list of available languages. In CODESYS, the selected language is displayed in the area “Localized Texts”. Use the “Text” column for typing the localized texts. |
). The layout from top to bottom corresponds to the layout displayed later in the