Function: Use this dialog for generating new toolbars or customizing existing toolbars.
Call: Main menu “Tools Customize” (“Toolbars”).
When you click “OK” to close the dialog, the changes are visible in the menu bar of the CODESYS user interface.
Display of currently defined toolbars. In CODESYS, the associated commands are listed below each toolbar in the order they will appear in the toolbar. Double-clicking a toolbar in the list switches to editing mode. |
|
“Add Toolbar” |
Enabled when a toolbar is selected. In CODESYS, this adds a toolbar above the selected toolbar and places the cursor in the name field of the new toolbar. |
“Add Command” |
Enabled when you select a command or blank command entry below a toolbar. Adds a command above the selected command. Opens the “Add Command” dialog. Use the “Add Command” dialog to select one or more commands. Left part: List of categories. Right part: List of commands in the selected category. |
“Add Separator” |
Adds a separator above the selected command. |
“Hide” |
Hide the selected toolbar from the user interface. |
“Show” |
Shows the selected hidden toolbar in the CODESYS user interface. |
“Reset” |
Resets the default settings of the toolbars. |
“Load” |
Loads the settings from a stored file (<file name>.opt.tbar). |