Function: This command opens the dialog “Project Archive” for the configuration of project archives.
Call: Menu bar: “File Project Archive”
An archive file (*.projectarchive) contains all files contained and referenced in the currently opened project. It can either be saved or dispatched as an e-mail attachment. The dispatch by email is very helpful for providing an employee with all project-relevant files. The file can be simply unpacked again with the command “Extract Archive”.




NOTICE

The archiving function is not intended for the storage of a project, but rather for the simple summarizing of all project-relevant files.
Dialog 'Project Archive'
The dialog displays all the categories that can be added to the project archive. In
this dialog, complete categories or individual objects from the categories can be
added to the project archive by setting a check mark (
).
Entries that are display as red in the list require your attention. Move the mouse pointer over this library for more information.
|
“Additional Files” |
Opens the dialog “Additional Files”. Here, further files can be added to the archive with the “Add” button. |
|
“Comment” |
Opens the "Comment" dialog. Here, comments can be added to the archive. |
|
“Save” |
Creates the archive file and saves it. The storage location and the archive name are specified in the subsequent dialog |
|
“Send” |
Creates a temporary archive file that is attached to an empty e-mail. A correct installation of the MAPI (Messaging Application Programming Interface) is required for the successful execution of this operation. Failure is documented by the display of a corresponding error message. The temporary archive is automatically deleted after sending the e-mail. |