Function: The command extracts a project archive, that was created with the command “Save/Send Archive”. You have to configure which objects of the archive CODESYS shall extract and in which directory of the file system they will be copied.
Call: Main menu “File Project Archive”
The file extension of an archive is .projectarchive
.
After the archive is selected, the dialog “Extract Project Archive” opens to configure the extract parameters.
Dialog Box 'Extract Project Archive'
This dialog box shows the contents of the project archive. You can exclude complete
categories or single objects from categories by clearing the check boxes () from the extraction.
“Extract into the same folder where the archive is located” |
The archive is extracted to the same directory. |
“Extract into the following folder” |
The contents of the archive are extracted to the given path. |
“Advanced” |
Opens the “Advanced” dialog box for you to define where special and additional files from the archive are extracted. |
“Items” |
Shows the contents of the archive structured in object categories.
|
“Comment” |
Comment that was entered when creating the project archive |
“Extract” |
If an extracted file has the same name as an existing file in the target directory,
then a dialog box opens, prompting whether the local file should be replaced. The
decision can be applied automatically to any additional conflicting names. In this
case, you have to select the |
Dialog 'Advanced'
“Install devices into” |
Drop-down list with currently available repositories. Select the repositories, in which CODESYS shall install the devices and the libraries of the archive. |
“Install libraries into” |
By default the "additional files" are set to “Do not extract”. Select the entries in the table and chose one of the following options: |
|
“Extract into project folder” |
Folder of the project file |
“Extract into folder” |
User defined folder |
“Do not extract” |
Default |
See also