You can configure a project archive and then save it in the file system or send it directly in an e-mail.
To send, follow the guide below as far as point 9. There, click on the button “Send” instead of “Save” in order to directly open the standard e-mail program, in which a new mail will automatically be created with the project archive file as an attachment.
Requirement: A project is opened.
-
Select “File Project Archive Save/Send Archive”.
The dialog box “Project Archive” appears.
-
Activate the checkbox next to each object that is to be saved in the archive.
In order to guarantee know-how protection,CODESYS will not automatically add unprotected libraries, not available as "compiled-library", to a project archive. If you explicitly select such a library in the list of additional files, you will get an appropriate warning.
-
If you want to pack further files in the archive, click on “Additional Files”.
The dialog box “Additional Files” opens.
-
Click on “Add”.
-
Select the files and click “Open”.
The files are added to the list of additional files.
-
Click on “OK”.
-
Click on “Comment”.
The dialog box “Comment” opens.
-
Enter a comment and click on “OK”.
-
Click on the button “Save”.
-
Select a storage location and a file name and click on “Save”.
The project archive is saved in the file directory.