Symbol: 
Function: The command numbers the elements so that the selected elements are located at the front of the execution order.
Call: Menu bar: “CFC Execution Order”; context menu: “Execution Order”
Requirements: A CFC editor is active and the “Explicit Execution Order Mode” property is selected. At least one element is selected.
The selected elements get the lowest numbers beginning at 0 while keeping the previous order. The remaining elements are numbered so that their execution order remains the same. The topological positions of the elements are retained anyway.