Symbol: 
Function: The command numbers the elements so that the selected elements are located at the end of the execution order.
Call: Menu bar: “CFC Execution Order”; context menu: “Execution Order”
Requirements: A CFC editor is active and the “Explicit Execution Order Mode” property is selected. At least one element is selected.
The selected elements get the highest numbers while keeping the previous order. The remaining elements are numbered so that their execution order remains the same. The topological positions of the elements are retained anyway.