Function: The command orders the execution order of the elements by their topological position from right to left and from top to bottom.
Call: Menu bar: “CFC Execution Order”; context menu: “Execution Order”
Requirements: A CFC editor is active and the “Explicit Execution Order Mode” property is selected. At least one element is selected.
The command applies to all elements in the program, even if not all elements are selected when the command is executed. The topological positions of the elements are retained anyway.