The operator is an extension of the IEC 61131-3 standard.




NOTICE

For compatibility, the compiler version must be >= 3.3.2.0.
The operator releases the memory of instances that the "__NEW" operator generated
dynamically. The __DELETE
operator does not have a return value and the operand is set to zero after this operation.
Requirement: The “Use dynamic memory allocation” option is selected on the “Application Build Options” tab in the properties dialog of the application.
__DELETE (<pointer>)




NOTICE

Two tasks should not call __DELETE simultaneously. Either you use a semaphore (SysSemEnter) or comparable method to prevent any concurrent calling of __DELETE , or you use __DELETE in one tasks only (recommended).
You can use a semaphore (SysSemEnter) to prevent two tasks from allocating memory
at the same time. As a consequence, the extensive use of __DELETE
causes higher jitter.
If Pointer
references a function block, then CODESYS calls the associated FB_EXIT
method before the pointer is set to zero.
Examples
FUNCTION_BLOCK FBDynamic VAR_INPUT in1, in2 : INT; END_VAR VAR_OUTPUT out : INT; END_VAR VAR test1 : INT := 1234; _inc : INT := 0; _dut : POINTER TO DUT; neu : BOOL; END_VAR out := in1 + in2; METHOD FB_Exit : BOOL VAR_INPUT bInCopyCode : BOOL; END_VAR __Delete(_dut); METHOD FB_Init : BOOL VAR_INPUT bInitRetains : BOOL; bInCopyCode : BOOL; END_VAR _dut := __NEW(DUT); METHOD INC : INT VAR_INPUT END_VAR _inc := _inc + 1; INC := _inc; PLC_PRG(PRG) VAR pFB : POINTER TO FBDynamic; bInit: BOOL := TRUE; bDelete: BOOL; loc : INT; END_VAR IF (bInit) THEN pFB := __NEW(FBDynamic); bInit := FALSE; END_IF IF (pFB <> 0) THEN pFB^(in1 := 1, in2 := loc, out => loc); pFB^.INC(); END_IF IF (bDelete) THEN __DELETE(pFB); END_IF