The operator is an extension of the IEC 61131-3 standard.
BITADR
yields the bit offset within a segment in a DWORD
.




NOTICE

The offset depends on whether the "Byte addressing" option is selected or cleared in the target system settings.
The highest value nibble (4 bits) in this DWORD
defines the memory range.
Marker M
: 16#40000000
Input I
: 16#80000000
Output Q
: 16#C0000000




CAUTION

When using pointers to addresses, note that applying an online change can shift the contents of addresses.
Example
ST implementation language
VAR xVar AT %IX2.3 : BOOL; dwBitoffset : DWORD; END_VAR dwBitoffset := BITADR(xVar); (* If byte addressing = TRUE, result = 16#80000013; if byte addressing = FALSE, result = 16#80000023 *)