SIZEOFPermalink

IEC operator: This function is not prescribed by the standard IEC 61131-3.

⮫ “Overview”

Perform this function to determine the number of bytes required by the given variable.

Example in ST:

‎var1 := SIZEOF(arr1);‎