OverviewPermalink

All IEC operators are supported. In contrast with the standard functions (see Appendix D of the Standard library), these operators are recognized implicitly throughout the project.

⮫ “Standard library”

Besides the IEC operators also the following operators are supported which are not prescribed by the standard: INDEXOF and SIZEOF, ADR and BITADR.

⮫ “Arithmetic operators”

⮫ “Address operators”

Operators are used like functions in POU.