| 
                                  This is the web edition of the original ⮫ AC500-S safety user manual, version 1.3.2. This web edition is provided for quick reference only. The original safety user manual must be used to meet functional safety application requirements.  | 
                           
The SF_MAX_POWER_DIP_GET_CFG function returns the configured maximum power dip value of the safety CPU.
| 
                                  Name  | 
                              
                                  Data type  | 
                              
                                  Initial value  | 
                              
                                  Description, parameter values  | 
                           
|---|---|---|---|
| 
                                  VAR_OUTPUT  | 
                           |||
| 
                                  SF_MAX_POWER_DIP_GET_CFG  | 
                              
                                  WORD  | 
                              
                                  16#0000  | 
                              
                                  Configured maximum number of tolerated power dips (undervoltage/overvoltage faults).  | 
                           
Call in ST
MAX_POWER_DIPS_CFG := SF_MAX_POWER_DIP_GET_CFG();