|
This is the web edition of the original ⮫ AC500-S safety user manual, version 1.4.0. This web edition is provided for quick reference only. The original safety user manual must be used to meet functional safety application requirements. |
|
Standards |
Requirements |
|---|---|
|
IEC 60204-1:2016 |
9.2.2: Stop function categories; category 0 |
|
ISO 13849-1:2015 |
5.2.1 Safety-related stop function A safety-related stop function (e.g., initiated by a safeguard) shall, as soon as necessary after actuation, put the machine in a safe state. 6.2 Specifications of categories Fault detection (of the actuator, e.g., open circuits) |
|
ISO 12100:2010 |
6.2.11.2 Starting of an internal power source/switching on an external power supply 6.2.11.4 Restart after power interruption |
|
ISO 13849-1:2015 |
5.2.2 Manual reset function |
External device monitoring (EDM): The FB controls a safety output and monitors controlled actuators, e.g., subsequent contactors.
General:
The SF_EDM FB controls a safety output and monitors controlled actuators.
This function block monitors the initial state of the actuators via the feedback signals (EDM1 and EDM2) before the actuators are enabled by the FB.
The function block monitors the switching state of the actuators (MonitoringTime) after the actuators have been enabled by the FB.
Two single feedback signals must be used for an exact diagnosis of the connected actuators. A common feedback signal from the two connected actuators must be used for a restricted yet simple diagnostic function of the connected actuators. When doing so, the user must connect this common signal to both parameter EDM1 and parameter EDM2. EDM1 and EDM2 are then controlled by the same signal.
The switching devices used in the safety function should be selected from the category specified in the risk analysis (ISO 13849-1).
Optional startup inhibits:
-
Startup inhibit in the event of block activation.
|
Name |
Data type |
Initial value |
Description, parameter values |
|---|---|---|---|
|
VAR_INPUT |
|||
|
Activate |
BOOL |
FALSE |
|
|
S_OutControl |
BOOL |
FALSE |
Variable. Control signal of the preceding safety FBs. Typical function block signals from the library (e.g., SF_OutControl, SF_TwoHandControlTypeII, and/or others). FALSE: Disable safety output (S_EDM_Out). TRUE: Enable safety output (S_EDM_Out). |
|
EDM1 |
BOOL |
FALSE |
Variable. Feedback signal of the first connected actuator. FALSE: Switching state of the first connected actuator. TRUE: Initial state of the first connected actuator. |
|
EDM2 |
BOOL |
FALSE |
Variable. Feedback signal of the second connected actuator. Depending on the actuators installed and the targeted safety level, it may be that only combined inputs are allowed for wiring the feedback signals. In that case the user must use a graphic connection to jumper the EDM1 and EDM2 parameters. EDM1 and EDM2 are then controlled by the same signal. FALSE: Switching state of the second connected actuator. TRUE: Initial state of the second connected actuator. |
|
Reset |
BOOL |
FALSE |
|
|
MonitoringTime |
TIME |
#0ms |
Constant. Maximum response time of the connected and monitored actuators. |
|
VAR_OUTPUT |
|||
|
Ready |
BOOL |
FALSE |
|
|
S_EDM_Out |
BOOL |
FALSE |
Controls the actuator. The result is monitored by the feedback signal EDMx. FALSE: Disable connected actuators. TRUE: Enable connected actuators. |
|
SafetyDemand |
BOOL |
FALSE |
Optional. |
|
ResetRequest |
BOOL |
FALSE |
Optional. |
|
Error |
BOOL |
FALSE |
|
|
DiagCode |
WORD |
16#0000 |
|
Function block-specific error and status codes
|
DiagCode |
State name |
State description and output setting |
|---|---|---|
|
C001 |
Reset Error 1 |
Static Reset signal in state 8401. Ready = TRUE S_EDM_Out = FALSE SafetyDemand = FALSE ResetRequest = FALSE Error = TRUE |
|
C011 |
Reset Error 21 |
Static Reset signal or same signals at EDM1 and Reset (rising trigger at Reset and EDM1 at the same time) in state C010. Ready = TRUE S_EDM_Out = FALSE SafetyDemand = FALSE ResetRequest = FALSE Error = TRUE |
|
C021 |
Reset Error 22 |
Static Reset signal or same signals at EDM2 and Reset (rising trigger at Reset and EDM2 at the same time) in state C020. Ready = TRUE S_EDM_Out = FALSE SafetyDemand = FALSE ResetRequest = FALSE Error = TRUE |
|
C031 |
Reset Error 23 |
Static Reset signal or same signals at EDM1, EDM2, and Reset (rising trigger at Reset, EDM1, and EDM2 at the same time) in state C030. Ready = TRUE S_EDM_Out = FALSE SafetyDemand = FALSE ResetRequest = FALSE Error = TRUE |
|
C041 |
Reset Error 31 |
Static Reset signal or same signals at EDM1 and Reset (rising trigger at Reset and EDM1 at the same time) in state C040. Ready = TRUE S_EDM_Out = FALSE SafetyDemand = FALSE ResetRequest = FALSE Error = TRUE |
|
C051 |
Reset Error 32 |
Static Reset signal or same signals at EDM2 and Reset (rising trigger at Reset and EDM2 at the same time) in state C050. Ready = TRUE S_EDM_Out = FALSE SafetyDemand = FALSE ResetRequest = FALSE Error = TRUE |
|
C061 |
Reset Error 33 |
Static Reset signal or same signals at EDM1, EDM2, and Reset (rising trigger at Reset, EDM1, and EDM2 at the same time) in state C060. Ready = TRUE S_EDM_Out = FALSE SafetyDemand = FALSE ResetRequest = FALSE Error = TRUE |
|
C071 |
Reset Error 41 |
Static Reset signal in state C070. Ready = TRUE S_EDM_Out = FALSE SafetyDemand = FALSE ResetRequest = FALSE Error = TRUE |
|
C081 |
Reset Error 42 |
Static Reset signal in state C080. Ready = TRUE S_EDM_Out = FALSE SafetyDemand = FALSE ResetRequest = FALSE Error = TRUE |
|
C091 |
Reset Error 43 |
Static Reset signal in state C090. Ready = TRUE S_EDM_Out = FALSE SafetyDemand = FALSE ResetRequest = FALSE Error = TRUE |
|
C010 |
EDM Error 11 |
The signal at EDM1 is not valid in the initial actuator state. In state 8810 the EDM1 signal is FALSE when enabling S_OutControl. Ready = TRUE S_EDM_Out = FALSE SafetyDemand = FALSE ResetRequest = R1 Error = TRUE |
|
C020 |
EDM Error 12 |
The signal at EDM2 is not valid in the initial actuator state. In state 8810 the EDM2 signal is FALSE when enabling S_OutControl. Ready = TRUE S_EDM_Out = FALSE SafetyDemand = FALSE ResetRequest = R1 Error = TRUE |
|
C030 |
EDM Error 13 |
The signals at EDM1 and EDM2 are not valid in the initial actuator states. In state 8810, the EDM1 and EDM2 signals are FALSE when enabling S_OutControl. Ready = TRUE S_EDM_Out = FALSE SafetyDemand = FALSE ResetRequest = FALSE Error = TRUE |
|
C040 |
EDM Error 21 |
The signal at EDM1 is not valid in the initial actuator state. In state 8810, the EDM1 signal is FALSE and the monitoring time has elapsed. Ready = TRUE S_EDM_Out = FALSE SafetyDemand = FALSE ResetRequest = R1 Error = TRUE |
|
C050 |
EDM Error 22 |
The signal at EDM2 is not valid in the initial actuator state. In state 8810, the EDM2 signal is FALSE and the monitoring time has elapsed. Ready = TRUE S_EDM_Out = FALSE SafetyDemand = FALSE ResetRequest = R1 Error = TRUE |
|
C060 |
EDM Error 23 |
The signals at EDM1 and EDM2 are not valid in the initial actuator states. In state 8810, the EDM1 and EDM2 signals are FALSE and the monitoring time has elapsed. Ready = TRUE S_EDM_Out = FALSE SafetyDemand = FALSE ResetRequest = R1 Error = TRUE |
|
C070 |
EDM Error 31 |
The signal at EDM1 is not valid in the actuator switching state. In state 8000, the EDM1 signal is TRUE and the monitoring time has elapsed. Ready = TRUE S_EDM_Out = FALSE SafetyDemand = FALSE ResetRequest = TRUE Error = TRUE |
|
C080 |
EDM Error 32 |
The signal at EDM2 is not valid in the actuator switching state. In state 8000, the EDM2 signal is TRUE and the monitoring time has elapsed. Ready = TRUE S_EDM_Out = FALSE SafetyDemand = FALSE ResetRequest = TRUE Error = TRUE |
|
C090 |
EDM Error 33 |
The signals at EDM1 and EDM2 are not valid in the actuator switching state. In state 8000, the EDM1 and EDM2 signals are TRUE and the monitoring time has elapsed. Ready = TRUE S_EDM_Out = FALSE SafetyDemand = FALSE ResetRequest = TRUE Error = TRUE |
|
C100 |
Init Error |
Similar signals at S_OutControl and Reset (R_TRIG at same cycle) detected (may be a programming error). Ready = TRUE S_EDM_Out = FALSE SafetyDemand = FALSE ResetRequest = FALSE Error = TRUE |
Definition for R1:
IF EDM_1 = TRUE AND EDM_2 = TRUE THEN R = TRUE ELSE R = FALSE
|
DiagCode |
State name |
State description and output setting |
|---|---|---|
|
0000 |
Idle |
The function block is not active (initial state). Ready = FALSE S_EDM_Out = FALSE SafetyDemand = FALSE ResetRequest = FALSE Error = FALSE |
|
8401 |
Init |
Block activation startup inhibit is active. Reset required. Ready = TRUE S_EDM_Out = FALSE SafetyDemand = FALSE ResetRequest = TRUE Error = FALSE |
|
8810 |
Output Disable |
EDM control is not active. Timer starts when state is entered. Ready = TRUE S_EDM_Out = FALSE SafetyDemand = TRUE ResetRequest = FALSE Error = FALSE |
|
8000 |
Output Enable |
EDM control is active. Timer starts when state is entered. Ready = TRUE S_EDM_Out = TRUE SafetyDemand = FALSE ResetRequest = FALSE Error = FALSE |