To integrate SCADA in Automation Builder software a zenon editor is used. The configured device network address and variables are synchronized with zenon editor to avoid double entry.
The Automation Builder supports both standard and multi-user functionality.
Application notes
The details on how to set up a communication between ABB Ability™ zenon SCADA system and an AC500 V3 PLC is described in the application note ⮫ AC500 V3 with zenon - AC500 driver.
Further, it's possible to setup AC500 V3 PLCs with HA Modbus TCP and communication with zenon using ABB AC500 driver. The procedure on how to use the High availability Modbus library is described in the application note ⮫ AC500 V3 with zenon - HA Modbus TCP connection.
The communication between zenon as OPC UA client with an AC500 V3 PLC as OPC UA server is explained in the application note ⮫ AC500 V3 with zenon - OPC UA connection.