With this command you open the dialog box for password assignment for user groups. This command can only be executed by members of group 0. When the command has been given, then the following dialog box appears:
In the left combobox 'User group' you can select the group. Enter the desired password for the group in the field 'Password'. For each typed character an asterisk (*) appears in the field. You must repeat the same password in the field 'Confirm password'. Close the dialog box after each password entry with 'OK'. If you get the message:
"The password does not agree with the
confirmation",
then you made a typing error during one of the two entries. In this case repeat both entries until the dialog box closes without a message.
Then, if necessary, assign a password for the next group by calling the command again.




WARNING

If passwords are not assigned to all user groups, a project can be opened by way of a group to which no password was assigned!
Use the command 'Object' 'Access rights' to assign the rights for single objects or all of them.
⮫ “'Project' 'Object access rights'”
Concerning the protection of a project see also the encryption of a project at project saving.