'Project' 'Add action'Permalink

This command is used to generate an action allocated to a selected block in the 'Object Organizer'. One selects the name of the action in the dialog which appears and also the language in which the action should be implemented.

⮫ “Object organizer”

The new action is placed under your block in the Object Organiser. A plus sign appears in front of the block. A simple mouse click on the plus sign causes the action objects to appear and a minus sign appears in front of the block. Renewed clicking on the minus sign causes the actions to disappear and the plus sign appears again. This can also be achieved over the context menu commands 'Expand Node' and 'Collapse Node'.

⮫ “'Expand nodes' 'Collapse nodes'”

⮫ “Action”