During runtime it might be necessary to update the firmware of the modules, e.g., for security reasons.
Updating the firmware and the application on a processor module is the same process than installing a firmware and an application on a very new processor module.
The installation can be performed either via a PC (recommended) or via a memory card.