PLC firmware/application updatePermalink

During runtime it might be necessary to update the firmware of the modules, e.g., for security reasons.

Updating the firmware and the application on a processor module is the same process than installing a firmware and an application on a very new processor module.

The installation can be performed either via a PC (recommended) or via a memory card.

⮫ “Firmware identification and update”

Fig. 27: The “Version information” tab of a device in the Automation Builder

FW_required_Version